FB#.IDENTIFIED

Description

This parameter reports the device type that the drive has successfully identified. Its value is based on FB#.SELECT.

Type

Description

Versions

Action Version Notes
Implemented 02-00-00-000
Feature Change 02-06-03-000 Added support for SSI feedback.
Feature Change 02-12-01-000 Added BiSS-B Digital types (35, 135).

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

FB#.SELECT

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.IDENTIFIED

3500h

23h

Unsigned8

-

-

Read only

No

FB2.IDENTIFIED

3501h

23h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30000

1

30000 (0x7530)

FB1.IDENTIFIED

Signed16

Read Only

Yes

30001

1

30001 (0x7531)

FB2.IDENTIFIED

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.IDENTIFIED

30000

Signed16

Read Only

-

FB2.IDENTIFIED

30001

Signed16

Read Only

-